Germany English
  1. Home
  2. Company
  3. Press Portal
 integrated portfolio for the needs-based automation of off-highway machines
 integrated portfolio for the needs-based automation of off-highway machines
Press release

A stringent approach from assistance to autonomy

Bosch Rexroth presents an integrated portfolio for advanced assistance functions and develops a future-proof platform

  • Ready-to-use: software modules and an intuitive HMI concept
  • Advanced: New assistance functions
  • Integrated: Ecosystem comprising software, sensors, HMI and telematics
  • Outlook: Control basis for autonomous and partly-autonomous functions

At bauma 2022, Bosch Rexroth will present an integrated portfolio for the needs-based automation of off-highway machines. The range comprehends assistance functions for excavators, wheeled loaders and telehandlers including advanced sensor systems and intuitive operating devices. These include driver assistance functions for more efficient working and even virtual walls and emergency braking assistants for greater work safety. Ready-to-use software modules help to reduce the integration time into existing and future vehicle architechtures and speed up their market launch. As a hardware platform for higher automation levels, Bosch Rexroth will announce a microprocessor-based, ROS2-compatible robotic control unit.

The future of construction, handling and municipal vehicles includes anything from high-performance assistance functions to fully autonomous operation. However, the complexity involved means that manufacturers of off-highway machines are faced with significant challenges. It is important to minimize not only the development outlay but also the technological, economic and legal risks.

The automation portfolio presented at bauma will be based on the proven BODAS kit for hardware, software and telematics. A good starting point are the BODAS AS software modules, in particular the ready-to-use ASRun modules for Rexroth control units (RC), which are easy to integrate. They can be adapted through parameterization and put into operation over the air (OTA).

Functions for greater productivity and safety

The current range of assistance functions for productive and safe working processes includes easier leveling, load capacity measurement during handling operations, electronic vibration damping and various motion control systems for wheeled loaders and telehandlers. Virtual walls and virtual rotary limiting systems protect the immediate surroundings by preventing the machine from accidentally leaving the safe working area. A number of functions can be adapted for other sectors, for example for tractor front loaders.

A groundbreaking HMI concept provides an intuitive user experience. It is based on ergonomic Sense+ joysticks with multidimensional optical and haptic feedback as well as high-resolution, high-contrast and glove-operable BODAS displays with easy-to-record visualizations for the relevant assistance functions.

The BODAS ecosystem also includes telematic modules for remote updates over the air (OTA), software remote maintenance and interfaces for transferring the wide range of operating data generated by the automation functions to ERP systems and their digital processes.

The new sensor systems for ultrasound, radar and inertial measuring systems form the basis for numerous other automation functions by recognizing objects in the surroundings and recording the position of the kinematic systems with respect to each other via acceleration. There are plans to add extra functions and sensors such as Lidar on a step-by-step basis.

The next generation of control units

With the concept of a processor-based robotic control unit, Bosch Rexroth gives an insight into the next generation of control hardware. In the future, it will serve as a standardized, high-performance control platform for higher levels of automation.

The need for high-performance, flexible control platforms is the result of the high computing power required for more automation. And in the future, the ability to develop, port and update software modules quickly and easily will become even more important. With a software architecture arranged in layers, the next generation of control units ensures that this is possible. They are based on Linux as the operating system and a clearly abstracted middleware layer and are compatible with the robotic operating system ROS2.

For object recognition and terrain mapping, Bosch Rexroth is working with Bosch to develop a ROS2-compatible perception stack. On this basis, Bosch Rexroth plans to offer complete function packages in the future – from sensor integration and object recognition to machine intervention.

The new control platform is currently being developed. Prototypes for pilot projects will be available from the middle of 2023.

Media Assets

Basic Information Bosch Rexroth

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 31,000 associates generated sales revenue of around 6.2 billion euros in 2021.

Basic Information Bosch

The Bosch Group is a leading global supplier of technology and services. It employs roughly 402,600 associates worldwide (as of December 31, 2021). The company generated sales of 78.7 billion euros in 2021. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. With its more than 400 locations worldwide, the Bosch Group has been carbon neutral since the first quarter of 2020. The basis for the company’s future growth is its innovative strength. At 128 locations across the globe, Bosch employs some 76,100 associates in research and development, of which more than 38,000 are software engineers.

Press Contact

Please get in touch with our Press Contact
Manuela Kessler - spokesperson technology topics

Spokesperson technology topics
Manuela Kessler
+49 9352 18-4145
Manuela.Kessler@boschrexroth.de

Related News

Agricultural and Forestry Maschines
Mobile Hydraulics
Construction Machinery

14/07/2023

New BODAS displays for mobile applications

Bosch Rexroth has expanded the BODAS ecosystem for mobile electronics with the new DI5 display range.

Read More
Mobile Hydraulics
Construction Machinery

21/06/2022

Best performance with maximum efficiency

Bosch Rexroth’s innovative electro-hydraulic and load sensing valve solutions provide users with high flexibility and configurability.

Read More
Mobile Hydraulics

21/06/2022

Up to 40 km/h without changing gear

With the A36VM, Bosch Rexroth presents an axial piston variable motor which is optimized for drivetrains. An increased swiveling range and a maximum pressure of 530 bar make mobile machines more efficient and quicker.

Read More