1. Home
  2. Company
  3. Press Portal
Hägglunds Quantum hydraulic motor range
Hägglunds Quantum hydraulic motor range
Press release

Efficient to the limit of performance

New Hägglunds Quantum motor range combines high performance data with sustainability and a long service life.

With the Hägglunds Quantum hydraulic motor range, Hägglunds removes previous performance limits in torque and speed and combines them with high efficiency. The direct drives can be used in heavy-duty applications as well as mobile applications.

Hägglunds Quantum hydraulic motors combine proven Hägglunds motor strengths such as high reliability with unique power density. With a maximum speed of more than 150 rpm and a maximum torque of more than 350 kNm, they offer a combination of torque and speed that is unique in the market. The engine achieves 3 MW corner power - without sacrificing compactness and efficiency.

“The Hägglunds Quantum range rewrites the rules of power density, especially when it comes to efficiency at higher speeds,” says Wolfram Ulrich, Vice President of Sales, Hägglunds. “By stretching the limits so far beyond previous solutions, it introduces possibilities for greener operation, mobile applications and more.”

Applications for which the Hägglunds CBp 280 motor was previously the most efficient solution can now use the Hägglunds Quantum Power 280, which is around 500 kg lighter. This saves resources and reduces emissions during production and transport. For mobile applications, this also means reduced weight and fuel consumption.

The Quantum range includes two motors. The Hägglunds Quantum is the new name of the Hägglunds CB, which has evolved significantly over time. Through optimizations in design and materials, Hägglunds Quantum has increased efficiency and tripled the average service life. The new Hägglunds Quantum Power, features an optimized design for outstanding efficiency and power density, developed with new simulation techniques. With additional connections and optimized channel geometries, this enables much higher speeds with full torque capacity and high efficiency. Both motors are suitable for crushers and internal mixers, for example, but also for mobile applications.

Bosch Rexroth at the HANNOVER MESSE: Hall 6, Booth D26

Media Assets

Here you can download the images from this Press Release

Basic Information Bosch Rexroth

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile and Industrial Applications as well as Factory Automation. With its intelligent components, customized system solutions, engineering and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries more than 32,000 associates generated sales revenue of around 7.0 billion euros in 2022.

Basic Information Hägglunds

Hägglunds stands for groundbreaking direct hydraulic drive technology and unswerving customer focus. Engineered and manufactured in Mellansel, Sweden, Hägglunds hydraulic motors and compact direct drive systems provide superior torque performance, flexibility and reliability to customers worldwide. Hägglunds is a brand of Bosch Rexroth, a leading global supplier of drive and control technologies. To learn more about Hägglunds solutions, visit www.hagglunds.com

Press Contact

Please get in touch with our Press Contact
Manuela Kessler - spokesperson technology topics

Spokesperson technology topics
Manuela Kessler
+49 9352 18-4145
Manuela.Kessler@boschrexroth.de

Related News

Assembly Technology
Industrial Hydraulics
Linear Motion Technology
Electric Drives and Controls

31/03/2025

Hannover Messe 2025

Bosch Rexroth presents future-proof hydraulics, open automation solutions and AI-based services at Hannover Messe.

Read More
Industrial Hydraulics

19/10/2022

The intuitive way to an energy-efficient pump drive: Size & Select Assistant for Sytronix

Whether in series and special machine construction or when retrofitting plastics processing machines: Variable-speed pump drives from the Sytronix family combine the benefits of hydraulics with maximum energy efficiency.

Read More
Industrial Hydraulics
Machine Tools (Forming)

12/09/2022

Plastics sector pioneers sustainable drive concepts

Manufacturers of plastics machines are traditionally pioneers for new drive concepts which improve performance and energy efficiency.

Read More