1. Home
  2. Showroom Mobile and Industrial World
Showroom Mobile & industrial World Showroom Mobile & industrial World

Mobile & Industrial World

We'd like to invite you to the Mobile & Industrial World, the special place being the part of our new showroom CU.BE. Everything, what is presented in the showroom CU.BE focus on exploring technologies, deepening the knowledge and finding the best way to create innovative solutions with benefits for users (CUstomer BEnefits).

In Mobile & Industrial World we present you exhibits, components and solutions, which are the overview of our new technologies in electrification, electrification, automation and saving energy in one place.

Visit us live or virtually

Find out more about presented solutions

In Mobile & Industrial World there are waiting for you e.g: eLION travel drive, a excavator equipped in BODAS, the travel drive eDA system, CytroBox, and an industrial technology demonstation machine. We hope that these will inspire you and help you realize your visions. Through meetings with our experts, you will learn how to improve system performance and make them more efficient while maintaining the highest quality standards.

  • Sensors and displays

    Sensors and displays

  • Compact hydraulics

    Compact hydraulics

  • Excavator

    BODAS control systems for mobile machines

  • Off highway system

    Off-highway vision system

  • Travel drive eDA system

    Travel drive eDA system

  • BODAS online

    BODAS online

  • eLION travel drive

    eLION travel drive

  • Industrial technology demonstration machine

    Industrial technology demonstration machine

Sensors and displays
Sensors and displays

Sensors and displays

SENSORS AND DISPLAYS

Very important elements in working machines are sensors. They provide not only the machine's safety, but also the operator's. Thanks to the sensors there is possibility of automation work of machines by controlling parameters e.g.: power, location, speed, air and oil temperatures, pressure etc.

DI5 DISPLAYS

Big screen solid displays, which can be used in different self-propelled machines. Products are freely programmable and very flexible. Thanks to their versatility, they can be used in every machine cabin, from forklift to bulldozer. Products from the DI5 family can be installed as a self-propelled device or integrated in a machine's dashboard. The 90 degree rotation causes the change of the image layout from horizontal to vertical or inversely. All the symbols can be read in every position, which restricts the number of necessary variants. The light sensor corrects the brightness of the display, and the lighting of all operation elements (color, intensity and day/night settings) can be configurate individual.

Compact hydraulics
Compact hydraulics

Compact hydraulics

The department of compact hydraulic systems uses a huge amount of resources to create the selling web canals, support engineering, research and service to deliver OEM products new, customized solutions and also to improve the service quality and cut the time of the product introductions to the market.

The stand shows compact hydraulics solutions, which offer mechanic and electromagnetic cartidge valves, valves in bodies, integrated hydraulic systems, compact directional valves and aggregates. These elements apply in: earthworks, cranes, basket lifts, agricultural machinery. Bosch Rexroth offers also elastic and dynamic configurator CHoose, which helps in easy way design hydraulic integrated system, compact directional valves, compact power units and hydraulic blocks.

Excavator
Excavator

BODAS control systems for mobile machines

Our solution assists the operator's functions thanks to ease in precisely finishing the area on every slope. This tool also helps in estimation of capacity while exploitation and restricts the movements in safety zones. The ride of working machines is possible thanks to the joysticks, which is optimized for the user's comfort with visual and tactile feedback elements, e.g. vibration of the joystick handle when approaching critical parameters or coordinates. Thanks to the new SENSE+ by Bosch Rexroth, joysticks are expanded by selling ergonomic and multifunctional control handles, which can be flexibly adjusted to variable requirements and many machine devices. The stand shows the hardware, software and IoT infrastructure. These three elements complement each other and offer a holistic look for automation of typical workflow and excavator's functions. BODAS supports the driver by helping him with routine tasks, making easier precise operation maneuvers like levelling the area. BODAS ensures increased safety.

Off highway system
Off highway system

Off-highway vision system

Sustainability and digitalization are the main development trends formative future market of working machines. Our solutions to electrification and automation working machines go to the future. Their aim is to provide efficiency and responsible usage of resources.

The Bosch Off-Highway Vision System provides a surround view of the environment of a working machine. The system helps drive the vehicle in a small and complex environment, where the field of view is often limited. Looking around all the time is a challenge, especially when reversing. Thanks to the Off-Highway Vision System, the machine operator sees clearly his surroundings. The solution ensures increase of safety, effectiveness, comfort and easiness of maneuvering. The latest technology ensures special accuracy and it can be used in different applications, like collision avoidance systems and machine automation.

THE WHOLE ENVIROMENT OF VEHICLE ON ONE SCREEN

A clear field of view is ensured thanks to four compact, wide angle cameras and digital process image. Collected images connect themselves and create the 360⁰ view from up on the current surround of the machine, which is displayed on the screen in real time. The system provides 14 different display modes.

Travel drive eDA system
Travel drive eDA system

Travel drive eDA system

The travel drive eDA system presents a ready-to-use, scalable travel drive system, which is realized by using a hydrostatic transmission. In this system are included components as hydraulic pump for closed system A4VG series 35 and hydraulic motors A6VM or MCR. Also on this stand are components creating a control system like the RC 5-6/40 controller and a set of PR4 pressure and rotational speed sensors. The solution was created for wheeled vehicles.

The travel drive system was designed basing on an eDA system and gives machines' producents the access to many safety functions and drive comfort, which so far, have often been a real problem to solve. By using the eDA system, the user has access to equipping the machine with functions like detecting the operator or diagnosing the hydrostatic system, but we also have a possibility of choosing up to 3 driving modes.

BODAS online
BODAS online

BODAS online

The BODAS stand presents possibilities of communication between hydraulic systems and their control. Also, it shows the communication of the whole system with the outside world thanks to our IoT solution — BODAS Connect. It allows doing many tasks, like checking the machine conditions, reading the error code or changing the work parameters. The presented on this stand controlling elements are fully programable in the programming language C and according to the IEC6113-3 standard in the CODESYS V3.5 environment. Used elements with appropriately selected control system provide getting high precise in controlling and appropriate level of machine safety. In addition, thanks to their compact sizes, they fit well into the design of the machine

eLION travel drive
eLION travel drive

eLION travel drive

The eLION travel drive presents the effective solutions by Bosch Rexroth to electrifying construction, agricultural, municipal and other mobile machines. The eLION platform delivers electric solutions for different functions in off-highway and special machines, independent on whether these vehicles are diesel, hybrid or fully electric. Individual components of eLION portfolio include not only trending in technical way high voltage motors and inverters, but also other high-performance components together with gear technology, hydraulics and software.

All eLION motors and inverters because of hard using conditions meet demanding standards. Components have an IP6K9K protection level. The range of work temperature is from -40°C to 85°C, and the up border for the motors, which has a current generator function, is 100°C. The resistance for shocks and vibrations of eLION components is accordingly 50g and 10g. Also, the producers and users can use implemented safety functions in the inverters, which are according to the ISO 13849 standard.

Industrial technology demonstration machine
Industrial technology demonstration machine

Industrial technology demonstration machine

The stand shows strenght and precision of hydraulic drive, and in conparision to electric drives, it is easily to show how little space is needed for a hydraulic system with an estimated strength. Thanks to this comparison, the differences between drives and the ease of controlling them are shown. The elements from which the stand was built are used in industrial applications, and the expanded safety system controls the state of all drives. By building this system as a complete stand, we can show not only individual products, but also their interaction in a real machine.

Learn about power supplies, supporting the system work in Mobile & Industrial World

Cytropac

CytroPac

Rexroth has started the hydraulic power unit revolution. Lack of installationspace is no longer a reason to go without hydraulic power: The new CytroPac power unit provides maximum power in the smallest space with everything you need for fast installation – including an economical Sytronix drive, completely wired frequency converter and Industry 4.0 compatibility. With powerful 4 KW and pressure of 240 bar in 50 percent less installation space. Furthermore, CytroPac also complies with the EU Ecodesign Directive 2009/125/EC. Simply connect power, fluid and interface and go. A small revolution!

CytroBox

CytroBox

The new CytroBox raises the level of production to the next higher plane. This newest generation of hydraulic power units for medium-range performance from 7.5 kW to 30 kW impresses with its intelligent combination of speed variability, synchronous motor and axial piston pump, which make the power unit even more efficient than comparable components. This is thanks to the ideal harmonization of servo motor and pump, as well as the needs-based energy consumption. Preset controllers in the variable-speed pump drives adjust the energy requirements of the machine to match the respective conditions. Consequently, the speed is reduced under partial or no load to save energy, and conversely increased under full load with a highly dynamic response. This speed control leads to energy savings of up to 80 percent in comparison to constantly driven power units.

Watch the video and explore the secrets of Mobile & Industrial World